Position Loop

Overview

The position loop is active when the drive operates in position mode (AXIS#.OPMODE = 2). The parameters that govern the position loop are shown in the Position Loop view. The various types of tuning inside AKD2G adjust these parameters, so you normally do not need to adjust the position loop parameters in the position loop screen.

Tabs in the Position Loop View

The position loop view includes an active block diagram. If you click on a block in the diagram, the appropriate tab opens below.

  • Gains. This tab shows the gains for the position loop.
  • Limiter. The value in the Maximum Position Error box (AXIS#.PL.ERRFTHRESH ) limits the position error (AXIS#.PL.ERR ) that can be present. When the maximum position error is exceeded, the drive generates fault F6001 , Following Error. If the maximum position error is set to 0 (default) then the maximum position error is ignored.

  • Status. This tab shows the present value of commanded position (AXIS#.PL.CMD ), position feedback (AXIS#.PL.FB ), position error (AXIS#.PL.ERR ), and velocity command (AXIS#.VL.CMD).

Position Loop Default Behavior and Changes

By default, only a proportional gain (AXIS#.PL.KP ) is applied in the position loop.

Position Loop Changes Based on Slider Tuning

Slider Tuning (see Slider Tuning) adjusts the proportional gain of the position loop (along with velocity loop view parameters; see Velocity Loop). If you adjust the bandwidthIn computer networking, bandwidth often refers to a data rate measured in bits/s, for example, network throughput. The reason for the connection of data rate with the term bandwidth is that the limit to the data rate of a physical communication link is related to its bandwidth in hertz using the slider tuner, then when you return to the position loop screen, you will see a change to the proportional gain only. No adjustment is made to the integral gain or feedforward gain through the slider tuner. The integral saturation levels are not applicable when the integral gain is set to 0. In the Gains tab, the boxes for these values may be populated with default values whether or not the integral gain is set to 0.

Related Parameters

AXIS#.PL Parameters

AXIS#.OPMODE

AXIS#.VL.CMD

 

 


Stay Connected with Kollmorgen

Copyright © 2018 Kollmorgen